Technical FAQs

Ask a Question

Why does the local/remote button not work on the ATV212 drive?

Issue:
Why does the local/remote button not work on the ATV212 drive?

Product Line:
Altivar 212, ATV212

Environment:
All

Cause:
N/A

Resolution:
From 0.0 press mode and arrow down to F---.
Enter and arrow up to F732.
Enter and make sure it is set to 0.
Was this helpful?
What can we do to improve the information ?