Technical FAQs

Ask a Question

How is the ATV61 derated to the next size rating?

Issue:
ATV61 is derated to the next size rating?

Product Line:
Altivar 61, ATV61

Environment:
All

Cause:
Drive going into an existing enclosure such as M-Flex, E-Flex, MCC.

Resolution:
Under main menu go to access level.
Set access level to expert.
Under drive menu, go into 1.4 Motor control menu.
Find Power identification and set it to IP00 (hold for 2 seconds).
Was this helpful?
What can we do to improve the information ?