Technical FAQs

Ask a Question

How can you remotely connect the VW3A1111 (Remote keypad) to the Altivar Process drive?

Issue:
How can you remotely connect the VW3A1111 (Remote keypad)  to the Altivar Process drive?

Product line:
ATV600, ATV900, Altivar Process

Environment:
all

Cause:
N/A

Resolution:
The VW3A1111 keypad has a cable port built into the bottom.  Move the rubber cover to access the port.  See the photo attached. 
This is generally a temporary connection.  To permanently remote mount the keypad, use VW3A1112.
 
Was this helpful?
What can we do to improve the information ?