Technical FAQs

Ask a Question

Data Center Operation | Video: How to configure IT Optimize?

Issue:
How to configure StruxureWare Data Center IT Optimize.

Product Line:
StruxureWare Data Center Operation

Environment:
StruxureWare Data Center Operation 7.5 and lower (Receiving Download Links and How to Install)
StruxureWare Data Center Operation 8.x (How to install only)

Cause:
How to configure StruxureWare Data Center IT Optimize.

Resolution:

Below is a video on how to configure IT Optimize?:



NOTE: This video shows both how to download and install ITO for Data Center Operation version 7.5 and lower. The configuration portion still applies to the Data Center Operation 8.x. If you need to receive the download links for ITO, please see the following knowledge base: ​FA297192
Was this helpful?
What can we do to improve the information ?