Technical FAQs

Ask a Question

Is a 110V I/O adapter available on Altivar Process drives?

Issue:
Is there a 110V Input Output card available for the Altivar Process drive?

Product Line:
Altivar Process drives, ATV600, ATV900

Environment:
All

Cause:
Information not available in current literature.

Resolution:
We currently do not offer a 110VAC or 120VAC digital input adapter card for the Altivar Process series drives.
Was this helpful?
What can we do to improve the information ?