Technical FAQs

Ask a Question

Is the VW3A1101 compatible with the ATV600 and ATV900 series process drives?

Issue:
Is the VW3A1101 compatible with the ATV600 and ATV900 series process drives?

Product Line:
ATV600 and ATV900 series

Environment:
All models, All serial numbers

Cause:
Information not available in current literature.

Resolution:
The VW3A1101 keypad is not compatible with the Altivar Process series drives.   It is only compatible with ATV61, ATV71, ATV212, ATV312, and ATV32 series drives.

The keypad part number for ATV630 & ATV930 process drive is VW3A1111.  An optional door mounting kit part number is VW3A1112.
Was this helpful?
What can we do to improve the information ?