Technical FAQs

Ask a Question

Can the Altivar 312 drive be powered up with an external control voltage?

Issue:
Can the ATV312 drive be powered up with external control voltage?

Product Line:
ATV312

Environment:
All serial numbers for ATV312

Cause:
To program the drive with external voltage

Resolution:
No, the VFD needs full supply voltage to power and program the drive. 
Was this helpful?
What can we do to improve the information ?