Technical FAQs

Ask a Question

Video: Why won't the ATV630 drive run in reverse?

Issue:
ATV630 won't operate in reverse.

Product line:
ATV600, ATV630, ATV650, Altivar Process

Environment:
All

Cause:
Configuring Reverse Motor Operation on Altivar 630 Process Drives

Resolution:
The Factory settings for the Process Drive to run in reverse is disabled in Reverse Disable parameter. 
Go to Complete Settings > Command and Reference > Reverse Disable, change the setting to No and save.  Now, you should be able to operate the drive in Reverse.

 
Was this helpful?
What can we do to improve the information ?