Technical FAQs

Ask a Question

What are the COM'X 210/510 natively supported devices?

Issue:
What are the COM'X 510 and Com'X 210 natively supported devices?

Product Line:
COM'X 510 (EBX510)
COM'X 210 (EBX210)

Environment:
Natively supported devices

Resolution:
Different firmware versions that run on Com'X devices supports different devices natively. The latest firmware supports a more completed list of devices natively. It's recommended to upgrade Com'X to latest firmware version to support more devices natively.

NOTE: Latest firmware for Com'X 510 can be downloaded here.  
           Latest firmware for Com'X 210 can be downloaded here

List of natively supported devices for different firmware versions can be downloaded here.
Was this helpful?
What can we do to improve the information ?