Technical FAQs

Ask a Question

What is the communications cable between the Magelis XBTN200 / XBTN400 and Modicon M221 controller?

Issue: 
What is the communication cable needed between an M221 and XBTN.

Product Line:
M221
XBTN200
XBTN400

Resolution:
Tthe communications cable between the XBTN400 and M221 is XBTZ9980
This is a Modbus RS485 communication cable.
Was this helpful?
What can we do to improve the information ?