Technical FAQs

Ask a Question

How can we regain some disk space on the HMIG5U?

Issue:
How can we regain some disk space on the HMIG5U?

Product Line:
HMIG5U,  HMIG5U2

Resolution:
One way to regain some disk space on the HMIG5U's CFast card is to disable the Hibernation feature in Windows.

To do so, start a command prompt and type the following:
powercfg -h off 

This will open up 3GB of free space on the CFAST card.

If the hibernation feature is required, then consider moving to the 32GB CFast system card.

 
Was this helpful?
What can we do to improve the information ?