Technical FAQs

Ask a Question

What services are required to be running for ION Enterprise, SPM, or PME system?

Issue
What steps are required to allow ION Enterprise, SPM, or PME to work properly after a reboot

Product Line
ION Enterprise 6.0.x
Struxureware Power Monitoring (SPM) 7.0.x
Power Monitoring Expert (PME) 7.2.x
Power Monitoring Expert (PME) 8.x
Power Monitoring Expert (PME) 9.0


Environment
Windows OS

Cause
Reboot required by customer

Resolution
Please refer to the attached excel document 'PME Service Matrix' for the PME Window Services Support Maxtrix:
Was this helpful?
What can we do to improve the information ?