Browse FAQs

Can we take the content from a File System Download and convert it back to a VDZ file so that we can make modifications in Vijeo Designer?

Published date: 05 June 2019

Issue:
Can we take the content from a File System Download and convert it back to a VDZ file so that we can make modifications in Vijeo Designer?

Product Line:
Vijeo Designer (all versions)

Resolution:
No, it is not possible to take the content from a File System Download and convert it back to a VDZ file so that modifications can be made in Vijeo Designer. The output of a File System Download is the compiled source of the project file. It is not possible to de-compile it, just like how you cannot obtain the source code from a .exe file in Windows.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.