Technical FAQs

Ask a Question

What would be the solution to connect a Magelis application using IEEE 1394 interface

Issue:
What would be the solution to connect a Magelis application using IEEE 1394 interface?

Product Line:
Magelis HMI, XBTGT, HMIGTO, HMIGTU, HMISTO, HMISTU series.

Resolution:
Today we have no such connection for the IEEE 1394 interface on the Magelis series of HMIs
 
Was this helpful?
What can we do to improve the information ?