Technical FAQs

Ask a Question

What faults can be reset with ATV61 or ATV71 automatic restart function turned on?

Issue:
What faults can be reset with ATV61 or ATV71 automatic restart function turned on?

Product Line:
Variable Frequency Drives

Environment:
Applies to Altivar 61/71

Cause:
Customer wants to know if he can automatically restart the drive after a fault 

Resolution:

Faults that can be reset with automatic restart function, after the cause has disappeared:
APF, CnF, COF, EPF1, EPF2, FCF2, Fd1, LFF2, LFF3, LFF4, nFF, ObF, OHF, OLC, OLF, OPF1, OPF2, OSF, OtF1, OtF2, OtFL, PHF, PtF1, PtF2, PtFL, SLF1, SLF2, SLF3, SPIF, SSF, tJF and ULF

NOTE: The drive must be set up for 2 wire control, 2-wire type set to level, be controlled by the drive's terminals, and the run command must be maintained in order for the Automatic Restart function to clear a fault and attempt a restart.  Also, the cause of the original fault must be resolved.


These faults that can be cleared by Automatic Restart are listed in the ATV61 and ATV71 Programming Manuals.

ATV61 Programming Manual:
https://www.schneider-electric.us/en/download/document/1760649/

ATV71 Programming Manual:
https://www.schneider-electric.us/en/download/document/1755855/
Was this helpful?
What can we do to improve the information ?