Technical FAQs

Ask a Question

Link 150 Device List option is missing when ION protocol is enabled

Issue
After enabling the ION protocol support in Link 150 (EGX150), the Device List is not shown anymore.

Product Line
EGX150

Environment
Gateway Protocol Support

Resolution

When the ION protocol is enabled, the following webpages are not needed which makes the options hidden:

Diagnostics → Device Health Check → Read Device Registers
Configuration & Settings → Network Configuration → Advanced Ethernet Settings
Configuration & Settings → Network Configuration → MBTCP/IP Filtering
Configuration & Settings → Device Configuration → Device List


 

Was this helpful?
What can we do to improve the information ?