Technical FAQs

Ask a Question

What analog inputs are available on the ATV630 Process Drive?

Issue:
What analog inputs are available on the ATV630 Process Drive?

Product line:
Altivar Process, ATV630, ATV600, Altivar 630

Environment:
All serial numbers

Cause:
n/a

Resolution:
The ATV630 drive comes with three analog inputs.  Each is programmable to be used for voltage or current.

The Min and Max Values are independently adjustable to allow setting up as voltage or current speed reference for most applications.  For example, 0-10V, 2-10V, 4-20mA, 20-0mA, etc.  
 
Was this helpful?
What can we do to improve the information ?