Browse FAQs

Where is the modbus serial communication port located on the Altivar Process Drive?

Published date: 09 May 2019

Issue:
Where is the modbus serial communication port located on the Altivar Process Drive?

Product Line:
Altivar Process Drive

Environment:
All serial numbers for Altivar Process Drive

Cause:
N/A

Resolution:
This drive has 2 RJ45 Communication Ports.  The Modbus Serial Communications Port is located on the control terminal card towards the right bottom. 
Reference picture below and document EAV64325

1 Modbus serial communication port



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.