Browse FAQs

What handles can be used with the GS2AH**F cable operator kits for GS2 Switches?

Published date: 01 August 2019

Issue:
Cable operator kit handle selection

Product Line: 
GS2 fusible disconnect switches

Enviroment:
UL 98 IEC Style Disconnect Switches

Resolution: 
These can use the 9422A1 to 9422A4 handles
NEMA type 1 3 3R 4 and 12 enclosures: 9422A3 (4 in handle depth) or 9422A1 (6 in handle depth) 
NEMA type 4 and 4X stainless steel enclosures: 9422A4 (4 in handle depth) or 9422A2 (6 in handle depth)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.