Technical FAQs

Ask a Question

If I use an ExRDM3913 motor with a Lexium SD328 drive, can I wire the motor thermistor to the SD328 temperature sensing terminals?

No, the temperature sensing circuit in SD328 will not function with the thermistor used in the Explosion Proof motor type EXRDM39xx.
The thermistor within ExRDM motors is not designed to be read by the temperature sensing circuit of Lexium SD3 type drives.

For temperature monitoring of the motor you must use a third party monitoring device as specified in the manual for ExRDM39 series motors.

Rev 11-3-17
 
Was this helpful?
What can we do to improve the information ?