Technical FAQs

Ask a Question

Is Java required for Power Monitoring Expert?

Issue
Will removing Java from the server negatively affect Power Monitoring Expert (PME) performance?

Product Line
PME 7.2.x
PME 8.x
PME 9.x

Resolution
For PME 7.2.x, Java is used by Floating License Manager version 1.3.1.  On a PME 7.2.2 system Java cannot be removed or PME licensing will no longer work. 

As of PME 8.x, the Floating License Manager no longer uses Java.  On PME 8.x and newer releases, Java can be removed without issue.
Was this helpful?
What can we do to improve the information ?