Technical FAQs

Ask a Question

What communication options are available on the Altivar 320 drives?

Issue:
What communication options are available on the Altivar 320 drives?

Product Line:
Altivar 320

Environment:
All serial numbers for Altivar 320

Cause:
N/A

Resolution:
Altivar Machine ATV320 drives with compact control block (ATV320-C) are equipped as standard with:
  • Integrated RJ-45 communication port for Modbus/CANopen
  • The VW3A3600 mechanical adapter can be ordered separately for use with communication modules for additional protocols, see the list below.

Altivar Machine ATV320 drives with book control block (ATV320-B) have been designed to simplify connections to communication buses and networks by means of the following:
  • Integrated RJ-45 communication port for Modbus/CANopen on the front
  • Slot for an optional communication module
The following optional communication modules are available:
  • Modbus TCP and EtherNet/IP (VW3A3616)
  • PROFIBUS DP V1 (VW3A3607)
  • DeviceNet (VW3A3609)
  • EtherCAT (VW3A3601)
  • POWERLINK (VW3A3619)
  • ProfiNet (VW3A3627)
Was this helpful?
What can we do to improve the information ?