Technical FAQs

Ask a Question

How to program an ATV630 (Process) drive to use a keypad as start/stop and AI1 as 4-20mA speed reference.

Issue:
How to program an ATV630 (Process) drive to use a keypad as start/stop and AI1 as 4-20mA speed reference.

Product Line:
Altivar ATV630

Environment:
All

Cause:
Programming

Resolution:
From main menu, go into to menu 5 (complete settings).
Scroll down to menu 5.5 menu (Command and reference)
Press OK and set Ref Freq 1 config to AI1.
Set control mode to separate.
Set Cmd channel 1 to terminals.
ESC back to Complete settings menu.
Scroll down to menu 5.11 Inputs/Outputs menu.
Go into AI/AQ tab.
Enter on AI1 configuration, and set analog input type along with min and max values as necessary.
Was this helpful?
What can we do to improve the information ?