Technical FAQs

Ask a Question

What is the Maximum Number of Memory Bits and Memory Word in M200 Controller.

- Nos. of maximum memory bits = 1024
- Nos. of maximum memory words = 8000
- Nos. of maximum double memory words / float points = 7999
- Nos. of maximum constant memory words = 512
- Nos. of maximum constant double memory words / float points = 511

Refer the attached document for more details
Was this helpful?
What can we do to improve the information ?