Technical FAQs

Ask a Question

Does IEC 60870-5-104 driver supports "Select Before Operate (SBO)" function.

Yes, SBO (Select Before Operate) is supported by  IEC 60870-5-104 protocol. Below are the details:
  • Direct command transmission
  • Direct set point command transmission
  • Select and execute command
  • Select and execute set point command
Was this helpful?
What can we do to improve the information ?