Technical FAQs

Ask a Question

Does Citect Anywhere Client require Remote Desktop Services (RDS) settings when running in the same machine in which Vijeo Citect is installed?

No, RDS settings are not required when Anywhere Client is running in same machine. In that case, only browser compatibility should be checked with Anywhere Client.
Was this helpful?
What can we do to improve the information ?