Technical FAQs

Ask a Question

How alarms can be logged in Text file which are saved in Vijeo Citect Project Directory named in format "YYYYMMDD.TXT".

Alarm logging is disabled by default and enabled by setting "Numfiles" to a value greater than zero value and the enterd value will determine the number of log files to be 
maintained. When this number is exceeded, Vijeo Citect deletes the oldest file. However, the user can retain logs by manually marking them as "Read Only". 
Add the below parameter to enable logging: 
[AlarmLog] 
NumFiles = 1 (or desired value upto 32767, default value is 0)

Logging for the above files will be in Text format and will be named in "YYYYMMDD.TXT" format.
Was this helpful?
What can we do to improve the information ?