Technical FAQs

Ask a Question

What is the accuracy of internal CT of Tesys T.

The internal CTs for the Tesys T are the protection class CT type 5P10. 

This means they can handle 10 times of the rated current with 5% accuracy without the CT getting saturated
Was this helpful?
What can we do to improve the information ?