Technical FAQs

Ask a Question

What is power dissipation of LC1DFK11P7

The Power dissipation of product LC1DFK11P7 is provided below 
- Power dissipation per pole in AC1 is 2,5 W 
- Average consumption of a.c. coil is 8 VA 
Consequently , the power dissipation is (2,5 x 3) + 8 = 15,5 W  
Was this helpful?
What can we do to improve the information ?