Search FAQs
How many expansion slots can be installed on the Altivar Process Drives?
Issue:
Expansion slots available with the Altivar Process Drives
Product Line:
Altivar Process Drives
Environment:
All serial numbers for Altivar Process Drives
Cause:
N/A
Resolution:
The Altivar 600/900 Process has 2 expansion slots:
Control electronic size does not change (even with 2 expansion cards used).
It is not possible to use the same expansion card twice and maximum one communication card is allowed.
Expansion slots available with the Altivar Process Drives
Product Line:
Altivar Process Drives
Environment:
All serial numbers for Altivar Process Drives
Cause:
N/A
Resolution:
The Altivar 600/900 Process has 2 expansion slots:
- Slot A (Right)
- Legacy communication options
- Advance Ethernet (only for ATV600)
- IO Extension Module (VW3A3203)
- IO Relays (VW3A3204)
- Slot B (Left)
- IO Extension Module (VW3A3203)
- IO Relays (VW3A3204)
- Encoder Module (only for ATV900)
- Slot C (Top) - (VW3A3800 - Only for ATV900)
- IO Extension Module (VW3A3203)
- IO Relays (VW3A3204)
- Safety option “premium” (VW3A3802)
Control electronic size does not change (even with 2 expansion cards used).
It is not possible to use the same expansion card twice and maximum one communication card is allowed.
Released for:Schneider Electric India
Explore more
Explore more