Technical FAQs

Ask a Question

Where can I download Ecostruxure Power Design - Ecodial ?

Ecostruxure Power Design - Ecodial is a Software - To "Design, calculate & size the equipment's" for your electrical installation.
The Electrical installation sizing is in accordance with Installation (IEC 60364) and Calculation standards(CENELEC TR50480).

Below we can see the links to download the latest INT version (V4.9) & the country versions on the same base line(v4.9). (localized versions are to meet the specific offer scope & the Language Translations)
Please copy & paste the required link from the below list.
 
Was this helpful?
What can we do to improve the information ?