Technical FAQs

Ask a Question

Data Center Operation | How to reset the command line Password?

Issue:
How to Reset the Password for Data Center Operation Server?

Product Line:
Data Center Operation (DCO)

Environment: 
Data Center Operation 8.x (DCO)

Cause:
If the password for logging into the Data Center Operation Server for either command-line console or the Webmin web interface is lost or forgotten.

Resolution:

To reset the password of Data Center Operation Server for either Webmin or the command line console please see the following DCIM Support article:

https://sxwhelpcenter.ecostruxureit.com/display/public/UADCO8x/Resetting+user+password+on+the+DCO+server
Was this helpful?
What can we do to improve the information ?