Technical FAQs

Ask a Question

What is the value at which the unit of Real energy change in PM2000 range.

Please find below value at which the unit of real energy will change:
a) 9999.9Wh >>> 10KWh 
b) 999.99KWh >>> 1MWh 
Was this helpful?
What can we do to improve the information ?