Technical FAQs

Ask a Question

Does the HMIG3U need a powered USB hub to power the XVGU and HMIZRA1?

Issue:
Does the HMIG3U need a powered USB hub to power the XVGU and HMIZRA1?

Product Line:
Magelis HMIG3U

Resolution:
No, the HMIG3U does not need a powered USB hub to power the XVGU and HMIZRA1. Each of the USB ports of the HMIG3U can supply upto 500ma of current. The two devices require 400ma each.
Was this helpful?
What can we do to improve the information ?