Technical FAQs

Ask a Question

What is the speed accuracy of ATV630 drive.

The speed accuracy is +/- 10 % of nominal slip in open loop.
 
Example: if the slip motor is 30 rpm, the maximum error of the ATV630 is of +/-3 rpm.
Was this helpful?
What can we do to improve the information ?