Browse FAQs

Can you run multiple motors with one ATV320 drive?

Published date: 06 December 2018

Issue:
Can you run multiple motors with one ATV320 drive?
 
Product Line:
ATV320
 
Environment:
Operating multiple motors simultaneously
 
Cause:
Documentation

Resolution:

Yes, but you need to size the drive according to the sum of the HP and max current of all the motors and provide separate overload protection for each motor.
All motors will will start/stop at the same time and run at the same speed.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.