Browse FAQs

How can you set up the ATV320 drive for modbus control and terminals control via HOA switch?

Published date: 15 September 2019

Issue:
Trying to setup an ATV320 drive for modbus control and terminals control via HOA switch.

Product Line:
ATV320

Environment:
All 

Cause:
LI1 will put the drive in terminal control and local wheel will be the speed reference.

Resolution:
LI1 FWD
L5 is REf switch and CCS switch
ref 1 modbus
ref 2 is LCC
Cd1 is modbus
Cd2 is terminal control
Profile is IO profile 

Jumper LI1 to LI5

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.