Technical FAQs

Ask a Question

Do I need to reconfigure 140NOC78100 module after a Hot Swap

You can replace the EtherNet/IP communication module at any time using another module with compatible firmware. A module can be replaced when power to the module is either:
  • off (cold swap), or
  • on (hot swap)
The replacement module obtains its operating parameters over the backplane connection from the CPU. The transfer occurs either immediately (hot swap) or when power is next cycled to the device (cold swap).
NOTE: The operating parameters that the CPU sends to a replacement module do not include any parameter values that were edited in the original module using explicit messaging "SET" commands. Explicit messaging can be performed in the Online Action window of the Unity Pro EtherNet/IP configuration tool. 
Was this helpful?
What can we do to improve the information ?