Technical FAQs

Ask a Question

Is there any compatibility table in Ecoreach which displays the overall firmware status of different modules in the IMU system.

When the ULP modules are upgraded with new functionalities, it is required to check the compatibility of the different modules in the IMU system. The Overall System firmware status table helps to diagnose and identify all discrepancy issues in the ULP modules. This table also provides the recommended actions relevant to the detected discrepancies.

NOTE: it is possible to perform this compatibility check only when the device is connected in Ecoreach.

Was this helpful?
What can we do to improve the information ?