Technical FAQs

Ask a Question

In Vijeo Citect, two tags are configured so that if one is ON, then other is OFF and events are logged to a DBF file. Double logging is happening every time in the DBF.

Set the Log Transition : OFF to False in the Alarm Categories if logging is not required if a particular alarm goes inactive.
After the setting, compile and run the project. 
By default, both are TRUE means it will log both states of an alarm.

Note : You can also set Log Transition : ON to False as per the requirement if logging is not required when alarm goes active.
Was this helpful?
What can we do to improve the information ?