Browse FAQs

What causes an IGBT overheating fault on the ATV630/ATV930 drive line?

Published date: 02 August 2019

Issue:
IGBT overheating fault on the ATV930 drive?

Product Line:
Altivar 930
Altivar 600
Altivar process

Environment:
All

Cause:
N/A

Resolution:
Verify the size of the load/motor/drive according to environmental conditions.
It is not recommended to have a motor/load be sized larger compared to the drive.
Check for proper cooling especially if the drive is located inside an enclosure such as MCC.
Check and or reduce switching frequency of the drive depending on application.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.