Technical FAQs

Ask a Question

Why is there an X over my driver under the IO Manager in Vijeo Designer?

Issue:
Why is there an X over my driver under the IO Manager in Vijeo Designer?

Product Line:
Vijeo Designer (all versions)

Resolution:
When there is an X over your driver added in your Vijeo Designer project, this can indicate that the driver files or Vijeo Designer was not properly installed. To resolve this issue, please re-install Vijeo Designer.
Was this helpful?
What can we do to improve the information ?