Technical FAQs

Ask a Question

After modifying a PowerSCADA Expert project, which steps must a user perform to make them active in Runtime.

Issue
After modifying a PowerSCADA Expert project, the user would like to know which steps must be taken to make them active in Runtime.

Product Line
PowerSCADA Operation 8.2
PowerSCADA Operation 9.0

Environment
PowerSCADA Expert Runtime

Resolution
 
Changes Being Made Compile Restart
Client HMI
Reload
Alarm Server
Reload
Trend Server
Restart
I/O Server
Stop and Start
Schneider Electric Core Service Host
Modify existing graphics pages including embedded Cicode Yes No No No No No
Add completely new graphics page(s) Yes Yes No No No No
Changes to PowerSCADA users (by using Cicode runtime CreateUser function) No No No No No No
Changes to Active Directory group membership No No No No No No
Changes to roles and Windows Active Directory group mapping Yes No No No Yes No
Changes to users and/or roles (by using the PowerSCADA Studio) Yes No No No Yes No
Changes to menu properties Yes No No No No No
Changes to server-side Cicode Yes No No No Yes No
Add/remove/modify alarm tags Yes No Yes No Yes Yes (if you need to update immediately)
Add/remove/modify trend tags Yes No No Yes No Yes (if you need to update immediately)
Add/remove/modify devices and/or variable tags Yes No No Yes No Yes (if you need to update immediately)

Note: The above table is intended for PowerSCADA Expert 8.2. You may use the table as a reference for previous versions, however there has been no testing to validate these recommendations. 
Was this helpful?
What can we do to improve the information ?