Technical FAQs

Ask a Question

How many finger-style vertical cable managers are required to fully populate one rail in a NetShelter cabinet?

Issue: 
Customers need to know how many cable managers are required to fully populate one or more rails in a cabinet. 

Product Line: 
NetShelter, vertical cable management. 

Environment: 
All versions and serial ranges. 

Cause: 
It is unclear how many cable managers are needed to fully populate one rail. 

Resolution: 
For all of the following skus, quantity 1 contains two cable managers that will populate one (1) vertical rail height: 
AR7580A
AR7585
AR7588
AR8442 
AR7721 
AR7722 
AR7723 
Was this helpful?
What can we do to improve the information ?