Technical FAQs

Ask a Question

What is the size of the PM8000's FTP site?

Issue:
What is the size of the PM8000's FTP site?

Product Line:
PM8000 series meters

Environment:
PM8000 FTP site memory

Cause
Unable to find the size of the FTP site memory

Resolution:
The FTP site for a PM8000 meter is approximately 350 MB in size.  This includes the directories for webpages, Comtrade, and IEC61850 files. The default webpages weigh in at around 5 MB. These can be removed to free up more FTP space, if required for custom web pages.
Was this helpful?
What can we do to improve the information ?