Technical FAQs

Ask a Question

Is Microsoft Office 365 supported with PME 8.x?

Issue:
A customer would like to know if PME 8.x is compatible with MS Office 365.

Product Line:
PME 8.x

Environment:
Software Compatibility

Resolution:
Currently PME 8.x supports Excel 2016 which is part of Office 365. This is strictly in the sense that Excel 2016 is installed locally on the server or engineering client in order to run reports.  The cloud based components of 365 are not supported.
Was this helpful?
What can we do to improve the information ?