Technical FAQs

Ask a Question

Is it possible to use PWS_DIAG function when BMXCPS4002 installed on BMEXBPxx00?

The BMXCPS4002 can be installed in BMEXBPxx00 or BMEXBPxx02, however no advanced diagnostics information is possible if you are not using BMEXBPxx02.
Was this helpful?
What can we do to improve the information ?