Technical FAQs

Ask a Question

Why doesn't my BMXART0814 work with my M580 processor but works for M340

Issue
The module won't go active at all. The fault in Unity says "module unserviceable".

Product Line
 M580

Environment
NA 

Cause
 The M580 requires SV2.xx minimum for this module. 
 
Resolution
Using the Unity loader, flash the attached firmware to the module. You would be needing a M340 plc to carry out this procedure. 
Was this helpful?
What can we do to improve the information ?