Technical FAQs

Ask a Question

We are not getting sp5606v1 I/O connection Equipment under I/O Connection Option in ISaGRAF Software.

There is only one variant is available for SP5606 equipment module. There is no V1 for this I/O module.

5606 input module measures current or voltage inputs in the ranges 0 to 20mA, 4-20mA, 0 to 5 V or 1 to 5 V. Each input is individually configured for input type and range. The 5606 module uses a 16-bit analog to digital (A/D) converter.

You can use SP5606 module only.
Was this helpful?
What can we do to improve the information ?