Technical FAQs

Ask a Question

Is EMC Certificate available for NSX MCCB Micrologic and BSCM ?

Currently we have only EMC certificates for the Micrologic trip unit of Compact NSX MCCB, not for the BSCM module. 
The Masterpact & NSX Micrologic conform to Class A EMC environment category as per IEC60947-2 standard.

EMC Certificate for Micrologic of Compact NSX MCCB's is attached herewith.

 
Was this helpful?
What can we do to improve the information ?